![](/media/12155/dubai_ida.jpg?anchor=center&mode=crop&width=520)
The event takes place 20 to 24 October in Dubai, United Arab Emirates (UAE). Danfoss will be present on booth 8.
In recent years, the number of desalination plants has increased along the coastlines of many continents. And the number is likely to continue to grow in the coming years as a natural response to the increasing water scarcity facing the world today.
The global water challenges call for innovative solutions and Danfoss is committed to supporting with expertise and unique technologies that can make SWRO solutions even more efficient without compromising the environment.
At IDA World Congress 2019, Danfoss exhibits four core technologies for efficient desalination: The APP high-pressure pumps, the iSave Energy Recovery Devices, the VLT® Aqua Drives and the new DST P40I pressure transmitter.
“Our target is to develop, manufacture and market innovative solutions for the demanding reverse osmosis (RO) market. We constantly work with our customers to make sure we meet the needs in the market”, says Jesper Bentzen Sales Director for Danfoss High Pressure Pumps.
Core technologies for various SWRO applications
High-pressure pumps, energy recovery devices, AC drives and pressure transmitters from Danfoss combine into sustainable and highly efficient desalination solutions that return substantial energy savings in both small containerized units up to larger trains of parallel-coupled pumps and ERDs.
“At IDA World Congress 2019, we will not only exhibit our APP pumps and iSave ERDs. We will introduce all four core technologies from Danfoss, and be ready to explain how you with the whole package can save up to 65% on energy costs”, Jesper Bentzen ends.
At the Danfoss booth you can explore the range of APP pumps used in more than 20,000 SWRO plants around the world to obtain maximum efficiency, reliability and flexibility in system set-up. You can learn more about the patented iSave ERD, scalable for use in SWRO applications of any size and type. You can also experience the Danfoss VLT® Aqua Drive, designed for maximum performance of water and wastewater systems with minimum energy consumption and the new Danfoss DST P40I titanium pressure transmitter, designed to meet requirements in corrosive environments as desalination systems.
Additionally, you can learn about the APP W HC pump recently released for ZLD/MLD industrial waste water treatment, built for outlet pressures of up to 120 bar and reducing energy consumption of ZLD/MLD plants significantly.
You will find us at booth 8, hall Sheikh Rashid, Dubai World Center, UAE.
More information about IDA World Congress 2019
About Danfoss
Danfoss High Pressure Pumps, member of the Danfoss Group, develops and manufactures axial piston pumps and isobaric energy recovery devices for demanding applications in a broad range of industries such as reverse osmosis. Danfoss Drives and Danfoss Industrial Automation, also members of the Danfoss Group, develop drives and pressure transmitters which among other things are suitable for demanding applications such as seawater RO. With tomorrow’s challenges within water scarcity, Danfoss is committed to innovation and has an eye on the future, Danfoss is engineering tomorrow.
Read more about our four technologies for desalination
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Decarbonizing within water treatmentDecarbonizing of water treatment comes down to energy efficiency
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }DesalinationDue to high energy efficiency and reliability, Sea Water Reverse Osmosis (SWRO) is one of the most sustainable and cost effective solutions for converting sea water to potable fresh water. Danfoss is committed to supporting the desalination industry with energy efficient SWRO solutions.