Energy efficiency is climate action

The greenest energy is the energy we don’t use. If we are to succeed in meeting global climate and energy goals, we need immediate action to curb energy demand.

Over 90% of global emissions are generated by buildings, transport, and industry [1]. Danfoss delivers one of the world’s strongest and most relevant portfolios of efficient components to these emission-heavy sectors. We engineer solutions that increase machine productivity, reduce emissions, lower energy consumption, and enable electrification. The solutions are available today to help accelerate sustainable transformation across these sectors.

Sustainable industries

The industrial sector is vital to achieving and maintaining a sustainable society. Heavy industries account for the vast majority of industrial emissions, and just steel, cement, and chemicals for more than half of industrial energy use and 70% of industrial emissions [2]. However, there is ample opportunity here to ensure energy is used only when needed. This can be achieved with highly efficient technologies that already exist today, such as a variable speed drive (VSD). 35% of all motors in the EU can benefit from a variable speed drive, and with a full implementation, energy savings of 121 TWh could be achieved [3]—a saving equivalent to 10% of the EU’s 2030 energy efficiency goals.  Additionally, if manufacturers were to install heat exchangers, they could produce more while using less – and even reuse energy by sending surplus heat back into the grid to warm our homes. 

15% energy savings with Danfoss Drives

Transport

The transport sector is still reliant on fossil fuels, procuring nearly 91% of its energy from oil – a 3.5 percentage points decrease compared to the early 1970s [4]. But electrifying transport does not just mean switching to renewable energy; it also means increased energy efficiency. 

For example, gas engines waste between 64% and 75% of the energy to convert power to movement, while the drive system of an electric vehicle reduces this loss to between 15% and 20% [5]. With heavy machinery and passenger ferries starting to go hybrid or fully electric, electrification is helping businesses achieve their green goals while lowering the total cost of ownership. 

Reducing emissions at sea

Buildings

The world is on course to build the equivalent of New York City every month for the next 40 years [6]. For every new square meter built, greenhouse gases are emitted during construction as well as when a building is heated, cooled, or filled with white appliances and devices. 

Today, buildings account for nearly 26% of the world’s energy-related emissions [7]. If we are to turn the tide, every square meter of new floor space needs to function using less energy. That means taking action anywhere we can. For example, by shifting a building’s energy consumption to the most economical period, digital flexibility solutions can ensure up to 20% savings in a building’s energy costs [8].

Decarbonizing buildings by enhancing energy efficiency
Hamburg residential area

Markets we serve

We deliver value to our customers as a global leading technology partner with deep application knowledge and sustainable innovation.

Get a complete overview of markets/sectors that we serve with our solutions.

  1. IEA (2020). Energy Technology Perspectives 2020. 

  1. Frauenhofer ICT (2023). Study on the energy-saving potential of electric motors with variable-speed drives in The European Union. 

  1. IEA (2022). Transport - Energy System - IEA. Accessed 27 February 2025 

  1. U.S. Department of Energy (n.d.). Where the Energy Goes: Electric Cars. Accessed 27 February 2025.   

  1. World Economic Forum (2024). Reducing Embodied Carbon in Cities | World Economic Forum. Accessed 27 February 2025 

  1. IEA (2023). Buildings - Energy System - IEA. Updated 11 July 2023. Accessed 27 February 2025. 

  1. Danfoss (2020). Optimize the indoor climate and cut down the costs. Published February 2020. Accessed 28 February 2025.