• My Apps
    My Apps You will have the option to use My apps once you login.

Best practices for trouble-free AC drive operation

Wednesday, February 7, 2018

When it comes to environments, there’s simply no telling where an AC drive will be installed. Installations in industrial applications can be some of the harshest.

Drives must be designed from the heatsink up, with many different applications in mind, and with the ability to deal with different climates, power sources, motor types and distances while being operated from a local control panel, fieldbus or discrete input/output (I/O). Not considering the environment from the beginning can result in a combination of increased maintenance costs, higher service costs, a decrease in operational reliability or, worst of all, more downtime.

In the past, this blog has brought you a series of posts that take a fairly detailed look into what kind of impact the installation environment can potentially have on your AC drive, and what are the appropriate precautions that can be taken to protect your investment. Topics included drives installed in locations with extremely low or high temperatureshumid or corrosive conditionshigh vibrations or in dusty environments.

This post, which assumes the drive is sized for appropriate control of the motor and application (voltage, power, response time and I/O needs), contains more best practices for trouble-free operation of your drive and application in the location in which it is installed.

Consider the following

  • Mechanical: is an enclosure needed for the environment in which the drive is installed?
  • Input power: what and how stable is the power source?
  • Motor wiring that powers the motor
  • I/O: wiring installed and routed to control the application
  • Fieldbus wiring for control and monitoring without interference

When selecting AC drives, many aspects are reviewed. The product must be able to drive the motor without interruption whether it runs for minutes, hours or 24/7, 365 days per year.

Ideally, an engineer could design the application from the ground up and all the necessary components would be considered, but this is often not the case. New installations in existing facilities, retrofits and upgrades take place every day. The following information helps provide the best opportunity for trouble-free operation.

Spacing

Space around the AFD allows air to circulate and around it for proper cooling. The manufacturer provides recommendations for space above, below and on the sides. In some instances, drives can be mounted side by side with no space around them.

Aggressive gases such as hydrogen sulfide, chlorine or ammonia can damage AFD electrical and mechanical components. Cooling air contamination can cause gradual decomposition of polychlorinated biphenyl tracks and door seals. A clear sign of an aggressive atmosphere is corroded copper. In aggressive atmospheres, enclosures and conformal-coated circuit boards are recommended. Read more about drives vs enclosure classes.

Power wiring

Input power – Distribution network, voltage and line disturbances

Understanding the power source (230, 460, 600 volts) is critical when selecting an AC drive. In some remote locations, only single-phase power is available, which requires a special design. In new designs, this information is readily available.

Key areas to investigate are:

  • Voltage level: select the appropriate drive for that voltage and single-phase or three-phase
  • Transformer configuration: does the transformer have a solidly grounded secondary? If not, the drive may have metal oxide varistors or filter caps that need to be removed.
  • Do power quality issues exist? This may require the use of a drive with a direct-current choke or line reactor built-in or the use of an external reactor or isolation transformer.

When wiring cables for input power, size wiring based on the AFD’s input current and comply with local and national electrical codes. Because these cables carry high voltage, they should be kept away from control wiring, other power wires and motor wiring to avoid inducing voltages in other cables.

Motor wiring – Grounding, shielding

The wire used between the drive and the motor should be reviewed. In a retrofit when replacing a starter or contactor with the drive, consider that motor wiring in the past may have been individual conductors in a conduit. AC drives use insulated-gate bipolar transistors to the drive output to control a motor and vary speed. The cable must be sized correctly and designed for its installation location. Along with the cable, the right drive and motor combination are needed. Consider if the environment has moisture, oil or potential for the cable to be crushed to select the appropriate cable and if a specific conduit is needed.

The best cable to use is one designed for AC drives. This cable will provide the necessary conductors for the motor: a ground and a shield. Grounding and the use of the shield are vital when it comes to higher-frequency switching at output terminals. Grounding is done for safety and provides a path from the motor back to the drive using single-point grounding. This means the ground conductor is connected at the motor and to the ground terminal on the drive. This single-point grounding technique is designed to keep the high-frequency noise generated between the drive and the motor so it does not spread to other equipment.

For drive installation on an older motor, an output reactor and a dU/dT filter are recommended to protect the motor from peak voltages that can occur at motor terminals because of reflected waves.

Induced voltage

Induced voltage from output motor cables that run together can charge equipment capacitors even with equipment turned off and locked out. Failure to run output motor cables separately or use shielded cables or metal conduits could result in death or serious injury. Remember to:

  • Run output motor cables separately or use shielded cables or metal conduits
  • Comply with local and national electrical codes for cable sizes
  • Follow the motor manufacturer's wiring requirements

Control wiring — Digital and analog I/O, Fieldbus, STO and encoder

Control wiring integrity is critical. The control wiring for digital and analog signals, fieldbus cables, safety circuits and feedback devices require shielded cables and separation from power and motor wiring. If control wiring needs to cross power or the motor, do so at a 90-degree angle.

Choose wiring designed for the signal carried, voltage and current rating. Use the shield to protect against crosstalk.

The cable from a remote, mounted control panel is often overlooked. This cable needs to be routed away from power and motor wiring as well.

Best practices

Manufacturer recommendations and manual instructions provide the best installation information and the best opportunity for trouble-free operation. If a deviation occurs, use the checklist below to run through each installation area. Some areas may not apply or can be changed because of cost or how and where they are installed. Try to reduce the amount of deviation from the manufacturer’s recommendations and follow local and national codes for installation and wiring.

Checklist

  • Additional equipment may be in the circuit with the drive. Make sure it is designed to operate with the drive and application. Look for power factor correction caps, line reactors or filters, disconnects or contactors. 
  • Test the function of I/O sensors or feedback sensors. 
  • Power, motor and control wiring need to be separated and proper spacing following within a cabinet. 
  • If wires cross, do so at a 90-degree angle.
  • Use conduits, wire trays or wire ties to separate the cables.
  • Look for broken or damaged wires and loose connections.
  • Check that control wiring is isolated from power and motor wiring for noise immunity.
  • Check the voltage source of the signals for proper levels.
  • Remove dust and debris from fans and heatsinks.
  • Make sure fans rotate.
  • Follow recommended spacing around the drive.
  • Understand the installation location and provide the correct enclosure, heating and cooling as needed for the product to properly operate.
  • Grounding is done for safety.
  • Follow applicable codes and ground the equipment following the manufacturer's guidelines.
  • Check for correct torque and that connections are free of corrosions, paints or coatings.
  • The input power needs to be sized according to current, voltage and environment (oil, water, vibration).
  • Follow all applicable electrical codes.
  • Check for loose connections and damaged wires (during preventive maintenance)
  • Route away from control wiring.
  • Motor leads need to be sized according to the current, voltage and environment (oil, water, vibration).
  • Route wiring to avoid inducing voltages in other cables.
  • Follow all applicable electrical codes.
  • Check for loose connections and damaged wires (during preventative maintenance).
  • Route away from control wiring.
  • Make sure the unit is mounted solidly or that shock mounts are used if necessary.
  • Check for equipment vibrations that could affect the drive.
  • Conditions change over time. Check equipment during preventive maintenance.

Keep following this blog for regular updates on the best ways to ensure that your investments in AC drives are always the safest investments around. Regardless of whose name is on the label, we’re here to help! In the meantime, you can find out more about all our products.

Author: Jim Kluck, Senior Product Marketing Manager, Danfoss Drives