![](/media/xzad20aw/1623909425330.jpg?anchor=center&mode=crop&width=520)
Master Follower Applications in the Mining Trade
Join Morten Juel Skovrup for a quick run-through of all the latest improvements and new features available in Coolselector®2. Plus, you’ll get to ask questions and get expert tips and tricks to get the most out of the software direct from its lead designer.
Variable Speed/Frequency Drives (VFD) are expanding their use as the starter of choice, not only in applications that require speed control but also in applications that require torque control and mechanical ‘soft starting’. The VFD has the capability to perform active load sharing between multiple motors on the same operating system, allowing one VFD to assume the function of a master and others as the follower, so when the master’s torque increases, the follower’s torque limit increases, allowing it to contribute more torque to the load.
Stop by on August 4th at 17:00 GMT+2 for: