![Powder mixing productivity triples with wireless PROFINET](/media/2315/f_b_cs4_profineta.jpg?anchor=center&mode=crop&width=520)
VLT® drives ensure accuracy at high speed, and deliver reliability so dependable that it’s decimated downtime.
A battery of 24 mobile mixers equipped with VLT® AutomationDrive FC 302 has revitalized the operations of the Dutch powder mix provider, Huijbregts Groep. Each mixer connects via wireless PROFINET to a PLC, which has dramatically improved process throughput, traceability, and operator safety. All with full reliability and at a very competitive price.