Succeeding in the competitive commercial real estate market in suburban Philadelphia is no problem for One Tower Bridge, a landmark 15-story office building located in West Conshohocken. Built on prime real estate between the winding Schuylkill River and bustling Schuylkill Expressway, the building was designed by one of the world’s leading architectural firms, Skidmore, Owings & Merrill.
But to keep its competitive edge, it was clear the owners had to replace the nearly 30-year-old HVAC units supplying the facility’s floor-by-floor variable-air-volume (VAV) system. The problem was that retrofitting with conventional packaged equipment or chillers would require removing windows, walls, and ceilings, compromising the elegant architecture. Instead, self-contained modular units employing Danfoss variable speed scroll compressors were able to fit through doorways easily, assemble quickly and operate quietly.
“We faced replacing fifteen 45-ton packaged HVAC units originally bought from Blazer Industries in 1988,” said John Sargent, building engineer for One Tower Bridge. “Transporting new, complete units to each floor was impossible. While the freight elevators are large, they certainly cannot transport a complete air-handling system. Removing windows or wall was also impossible. So, we were searching for a modular replacement unit that could fit our space restrictions and meet our particular performance requirements.”
Considering self-contained HVAC for VAV
The One Tower Bridge building offers 270,000 square feet of office space for tenants ranging from investment banking to healthcare firms.
To meet their comfort needs, the facility employs floor-by-floor, self-contained HVAC units for a VAV system.
With a VAV system, each unit supplies conditioned air to terminal units, small metal boxes located in the supply air duct just before the outlet diffuser. The terminal units in One Tower Bridge use pressure-independent sensors that control a damper which regulates maximum and minimum volumes of conditioned air supplied to the space. For comfort, the settings in each self-contained unit and each terminal can be adjusted to meet specific needs of tenants and the building owner.
That’s important to tenants in One Tower Bridge, because—contrary to the popular television series—it’s not always sunny in Philadelphia. In fact, Philadelphia experiences wide swings in temperature and humidity. The result is many hours when an HVAC system must adjust to changing indoor and outdoor environments, functioning in “partial load” conditions that challenge systems primarily designed for maximum efficiency on the hottest days at “full load” conditions.
Another variable: Like many buildings, One Tower Bridge is exposed to significant amounts of sunlight on two sides of the structure, creating an imbalance in solar heat gain between the south and north sides.
To meet these challenges, the building originally used self-contained, water-cooled HVAC units developed by Blazer Industries for VAV using reciprocal compressors. But now, 30 years later, the original units were difficult to maintain due to unavailable parts and costly R-22 replacement refrigerant. Moreover, it was clear that technology of the 1980s couldn’t meet 2020’s efficiency and performance
expectations.
Mechanically-modulated capacity scroll compressor capacity and noise were too much
In 2015, One Tower Bridge replaced a couple of the original units with a self-contained design using mechanically-modulated capacity scroll compressors. One new unit was installed on floor five, another on floor nine. Currently in operation, each unit contains two mechanically-modulated capacity and two conventional scroll compressors.
To handle varying loads, the units are configured to operate in two stages. Staging is split down the middle—the first stage runs two mechanically-modulated capacity scrolls, one on each of the left and right sections; the second stage runs a conventional fixed-speed compressor located in each section.
However, this solution proved less than ideal. To begin with, units were oversized. Only 60-ton units were available from the manufacturer instead of the required 45 tons. Consequently, during stage two,
compressors were going off on alarm due to overcooling. As a workaround for the overcapacity, hot gas bypass was added to the stage two compressor circuit, which was costly and reduced efficiency.
Another issue was noise. During stage one operation, the mechanically-modulated capacity scroll compressors emitted a disruptive sound that couldn’t be blocked by acoustic blankets.
Variable speed compressors adjust to the challenges
Fortunately, Sargent learned about a more advanced solution that could better handle the capacity, efficiency, and noise challenges.
“In 2016, I became aware of a manufacturer offering modular units—United CoolAir located in nearby York, Pennsylvania. When John Sargent and I toured their plant, we immediately saw their new VariCool EZ-Fit® self-contained modular unit was a better solution,” said Robert Miller of Coward Environmental Systems, the manufacturer representative providing One Tower Bridge’s mechanical systems.
United CoolAir was able to eliminate the first problem: oversizing. That’s because the VariCool EZ-Fit product line ranges from 12 to 90 tons, so a 45-ton selection was available.
Second, the technology is engineered specifically for floor-by-floor VAV retrofit projects. The system is designed in three distinct sections that easily mate to form a system module. Single modules are comprised of a fan, an evaporator coil, and a condensing section. For this application, one module supplies the north side, and another module the south side of the building.
The sections were completely assembled during manufacturing, charged with R-410A refrigerant, run tested, and then separated for shipment.
Third, the design’s customizability made it possible to build a far better solution. For this application, key components included electronically commutated motor (ECM) fans and Danfoss inverter scroll compressors VZH with CDS 303 variable frequency drives.
In November 2017, two VariCool EZ-Fit modules were installed—one for each side of the third floor. Each module employs one 25-ton Danfoss variable speed compressor VZH on one circuit and a conventional single speed scroll compressor on the other three circuits, each cycling sequentially as more capacity is needed.
For many applications, this staging configuration provides balanced air temperatures. However, given the differences between the north and south sides of One Tower Bridge, the air supplied to the outlet terminals benefited from further tweaking.
In November 2017, VariCool EZ-Fit modules using a slightly different configuration were installed on the first floor. Each of these modules employs one 25-ton variable speed scroll compressor VZH on the first and third circuits and a fixed speed 20-ton scroll compressor on the second and fourth circuits.
Stage one cooling activates the two variable speed compressors, stage two cooling runs the regular scroll compressor, then stage three cooling runs all four compressors.
By adding a second variable speed compressor, the design enables a 4:1 turndown ratio for optimum capacity control. As a result, the unit efficiently handles mild weather requiring as little as 25 percent cooling capacity—but can ramp up to 100 percent capacity on the hottest days.
This is accomplished by using three cooling stages with variable speed compressors VZH in conjunction with variable frequency drive fan speed control that meets ASHRAE 90.1 requirements.