• My Apps
    My Apps You will have the option to use My apps once you login.

How does district heating work?

Environmentally friendly and energy efficient heating supply

Environmentally friendly and energy efficient heating supply

Due to simultaneous production of heat and electricity in combined heat and power plants, district heating is very energy-efficient. By implementing renewable energy sources and utilizing waste heat generated by industry, the environmental gain by district heating is further evident. This kind of energy utilization is beneficial for both environment and society in general.

Compared to individual heating systems, the district heating plants are better at reducing emissions of hazardous compounds since they have more advanced pollution control equipment and through their more controlled conditions when generating heat. Furthermore, district heating is very convenient for consumers - who hardly notice how their radiators and tap water are heated on a daily basis.

District heating enables a green future

District heating enables a green future

District Heating is not only compatible with renewable energy sources of today; With an established district heating network, future energy sources can also be utilized centrally and distributed to consumers through existing district heating pipes.

Add to that supreme efficiency and the ability to utilize waste heat from electricity production and you have a system that is potentially the cornerstone of the future energy supply.

Renewable energy – substituting fossil fuels with sustainable alternatives

Renewable energy – substituting fossil fuels with sustainable alternatives

In pace with increasing environmental concerns, renewables have become a key issue. The flexibility of district heating allows for substitution to environmentally friendly alternatives.

Renewable energy is energy generated by natural resources and includes geothermal energy, biomass, wind energy, water energy, solar energy etc.

It is greenhouse-neutral. This means that it does not increase the concentration of greenhouse gases (e.g. CO2, methane, nitrous oxide and CFC) in the atmosphere.

These alternative renewable energy sources are compatible with district heating either directly or indirectly. Energy sources which are usually utilized in electricity generation such as water and wind energy are rarely used in district heating systems, but the majority of renewables are used to a high degree in district heating.

Contact us to learn more...