• My Apps
    My Apps You will have the option to use My apps once you login.

Danfoss honors EMCOR Services Mesa Energy Systems with sixth annual EnVisioneer of the Year award

Friday, September 25, 2015

Variable speed, oil-free, magnetic bearing technology results in some Mesa Energy Systems clients reporting reduced energy consumption and costs, substantial utility rebates, and lower payback periods.

Danfoss today announced EMCOR Services Mesa Energy Systems, of Irvine, Calif., is the winner of the sixth annual EnVisioneer of the Year award.

Launched in 2010, the EnVisioneer of the Year award competition recognizes North American end users, municipalities, building owners or original equipment manufacturers that have introduced a new product, opened a new facility or invested in a building or system upgrade using Danfoss products or solutions to realize significant energy and/or environmental savings.

EMCOR Services Mesa Energy Systems, a licensed commercial HVAC contractor offering HVAC maintenance and services, building automation systems, commercial refrigeration repair and chiller services, has used energy-efficient variable speed, oil-free, magnetic-bearing technology in a variety of retrofit applications, including the MacArthur Plaza commercial office building in Irvine, Calif. To combat increasing maintenance and energy costs in the nine-story, 154,530-square-foot structure, Mesa Energy Systems replaced 400 tons of existing reciprocating compressors with six oil-free centrifugal compressors. In addition to boosting the HVAC system’s cooling capacity to 500 tons, the solution also provided the flexibility to operate efficiently at loads ranging from 50 to 500 tons. The new system dramatically reduced energy consumption, resulting in the building owner reporting energy savings, a shortened payback period, and the acquisition of utility incentives. The system design and implementation also won the ASHRAE Southern California Technological Design Award.

Mesa Energy Systems also has experienced similar success in other retrofit projects using energy-efficient variable speed, oil-free, magnetic-bearing technology, including in a data center for a worldwide telecommunications provider that included the installation of eight 300-ton air-cooled chillers using oil-free centrifugal compressors. In combination with new chilled water pumps, flow meters and DDC controls, the data center reported substantial energy savings and utility incentives, which they cited as contributing to a payback period of less than three years.

“These examples reflect EMCOR Services Mesa Energy Systems’ winning approach to energy efficiency, especially in the retrofit market,” said Lisa Tryson, director, corporate communications, Danfoss. “They prove that, when properly applied, innovative technology can breathe new, more energy-efficient and cost-effective life into old buildings and produce impressive results.”

The EnVisioneer of the Year Award was presented on September 17 to Robert Lake, president and CEO, and Charles Fletcher, executive vice president, EMCOR Services Mesa Energy Systems, by John Galyen, president, Danfoss North America, Ricardo Schneider, president, Danfoss Turbocor® Compressors, and Tryson.

“We are pleased to recognize EMCOR Services Mesa Energy Systems with the EnVisioneer of the Year award,” said Galyen. “The first contractor to receive this award, Mesa consistently demonstrates the ability to retrofit buildings with principles that align with our global Engineering Tomorrow commitment – delivering quality, reliability and innovation and helping customers prepare to meet future climate and energy regulations. The work they do, including that using innovative and energy-efficient variable speed, oil-free, magnetic-bearing technology, and the energy savings clients report their work achieves contribute to significant reductions in utility bills and shorter payback periods for EMCOR customers.”

The EnVisioneer of the Year competition is judged and the winner is chosen by an independent third party.