Consumer retail stores are looking for tried-and-true ideas to thrive in turbulent economic times. That's why a major 190-store retail chain based in the Midwest switched to a proven refrigeration solution for one of its distribution centers -- an environmentally friendly ammonia system that uses Danfoss ICV Flexline valve stations.
"Ammonia is still the refrigerant of choice for large cold storage facilities," says Tom Cooper, president of Refrigeration Concepts, Inc., (RCI) Comstock Park, Michigan. "It is a naturally occurring gas that is environmentally friendly with an ozone depletion potential (ODP) and a global warming potential (GWP) of zero. Ammonia also has good thermodynamic properties that make it very energy efficient. And thanks to its long history, our industry knows how to handle it safely."
Looking into the future, the retail chain made a pro-active switch to a more environmental friendly refrigerant than the refrigerant they were using.
"Ammonia has a better Coefficient of Performance (COP) than typically installed halocarbon refrigerants," explains Cooper. "That makes it an efficient choice for a wide variety of temperatures and applications -- like refrigerated dock doors and blast freezers."
Cooper's challenge was to convert a 75,000-square-foot cold storage facility in Lansing Michigan requiring -10 degree F refrigeration for frozen meats and vegetables from HCFC-22 to ammonia utilizing existing penthouses and maintain temperatures during the process of demo and reconstruction.
Responsible for designing and installing the entire refrigeration system -- from compressors to condensing and evaporator coils -- Cooper's crew had to use some ingenuity because the project schedule was tight.