Danfoss Industries Pvt. Ltd. an industry leader in energy-efficient solutions for refrigeration, HVAC, heavy industries and district energy, today unveiled 6 new innovative products from its Cooling Segment at RefCold India, 2019 held at Hitex Exhibition Centre, Hyderabad. These products are set to change the standard of applications for the industrial refrigeration and cooling industry. The products were launched by Arvind Surange, Sr. Consultant for Cold Chain in the presence of a few esteemed customers, Danfoss representatives and several other industry dignitaries.
The products launched are - Danfoss Intelligent Purging System (IPS)/Air Purger; Danfoss Gas Detector; Danfoss Plate Heat Exchanger; EKE 400; IFCD Defrost Module; ICSH 2 Step Solenoid Valve.
Speaking on the launch, Mr. Ravichandran Purushothaman, President, Danfoss India said, “We at Danfoss invest heavily in increasing the momentum of our innovation through active R&D and on delivering technologically advanced products & solutions which help in promoting energy efficiency and sustainable development. With our new Cold Chain products, we are also focusing on the government’s goal of providing an integrated vision towards cooling across sectors, encompassing inter alia transition to natural refrigerants, enhancing the energy efficiency, safety, reliability and better technology”.
Mr. Carlsten Dahlgaard, Senior Director - Global Sales Development, Industrial Refrigeration, said, “It gives me immense pride as these products will drive the next wave of change in the industry. Danfoss believes in science-led innovation and these products are a testimony of the intellectual passion of our teams which have worked hard to make this launch possible for our customers.”
Commenting on the launch, Mr. Anuraaga Chandra, Head - Cooling sales, India said, ’’This is yet another milestone for us, at Danfoss as we unveil our new launches that are sure to transform the business of our clients while adding great value. The industry is at the helm of a massive technological advancement and we are hoping to continue crafting many such transformational products and solutions in the coming days.’’
Product note:
The Danfoss Intelligent Purging System (IPS) is an automatic, self-contained operating unit that helps remove non-condensable gases in a safe, energy-efficient and environmentally friendly way for industrial refrigeration systems. This helps maintain an optimum refrigeration capacity and system efficiency, allowing professionals to achieve maximum system performance.
The Danfoss Gas Detectors (plug and play gas detectors) are based on a digital platform that delivers improved operational reliability, easy calibration and maintenance efficiency, cost-effectiveness, and regulatory compliance for application in industrial refrigeration.
The Danfoss Plate Heat Exchanger (semi-welded plate heat exchangers) are optimized for industrial applications such as Condensers, Flooded and Pumped Evaporators, Sub-Coolers, Desuperheaters, Superheaters, Economizers and Oil Coolers.
The EKE 400 is an application for industrial refrigeration applications that can control the operation of the valves and the fans for evaporators to achieve optimal cooling mode and defrost sequence for an efficient, safe and trouble-free operation of the evaporators.
The ICFD is a product specially designed to improve defrost performance and reduce energy consumption for industrial refrigeration applications.
The ICSH 2 Step Solenoid Valve for safe and soft gas injection is a very efficient and common method used within industrial refrigeration. It is specifically designed keeping in mind the safety risks involved in injecting hot gas into evaporators.