Danfoss Cooling has supported 12 Adélie Penguins with a new gelid home in "Antarctica: the Kingdom of Penguins" at the Zoo in Guadalajara, Jalisco, Mexico. To permanently host a group of 12 Adélie Penguins (six males and six females of reproductive age), from a zoo in Japan is quite a project. Read what it takes to create a pleasant home for the flightless birds used to living in much colder areas of the world.
In April, the Zoo began the search for a provider that could adequately match the required areas for the penguins: a quarantine zone, the area of the public, the habitat of the penguins, a space to serve as a bedroom during the night and an ice machine.
According to Eduardo Luna, Sales Manager, Danfoss Refrigeration and Air Conditioning Distribution, "the Zoo opted for Danfoss solutions, due to several factors; one of them is the immediate availability of the equipment, allowing the twelve penguins were in observation during a period of quarantine, to rule out problems of health or adaptation before being displayed."
The quarantine area had a volume of approximately 80 m3 and should be stored at a temperature of zero degrees centigrade. This climate is maintained thanks to a sealed unit with a micro channel 5 HP and two evaporators. In that same area stood a 10.5 m3 swimming pool, which was kept refrigerated with another similar unit.