• My Apps
    My Apps You will have the option to use My apps once you login.

Globe valves

  • Overview
  • Documents
  • Tools and apps
  • FAQ
  • Case studies
  • Videos

The Danfoss motorized control valves range (MCV) for district heating is applicable for use in water and glycol-based heating and cooling systems.

The motorized control valves ensure stable and accurate control of water. This in turn improves temperature control, leading to enhanced comfort for the end-user. The motorized control valves range comprises both regular and pressure-relieved control valves operating with high differential pressure.

In energy efficiency terms, optimal performance of temperature control can lead to decreasing heat loss and therefore reduced CO2 emissions.

Good control ratios and rapid response times to changes in domestic hot water supply requirements are just some of the features needed to ensure optimum control performance.

The range of globe valves stands for progress in a number of essential areas, which meet the increasingly stricter requirements for control performance, features, compact design and price/value ratio. 

The valve series is available in different materials, which fulfill the heavy-duty requirements, and is supplied with different connections. Today we are able to offer a range of seated valves for use in the above-mentioned applications.

Features and benefits

Excellent control performance in meeting the most difficult control requirements in district heating, while still providing instantaneous hot water

Easy selection, installation, commissioning and maintenance lead to cost, time and effort savings

Built-in thermic and overload protection of the electromotor radically reduces the risk of operational failure in either the valve or the system as a whole

Documents

Documents
Type Name Language Valid for Updated Download File type

Tools and apps

Application guide

FAQ

At the same dp over the valve, we can close the pressure relieved valve with much lower force. The real benefit is that in most cases we can offer one actuator for the whole valve range.

The rangeability of a control valve expresses how stable the control characteristic of the valve is. Rangeability is a measure of the minimum controllable flow the valve is able to handle. It is defined as the ratio of maximum controllable flow to minimum controllable flow at a constant pressure drop. The higher a control ratio of a control valve, the better the control capability of the valve.

We have this information in our data sheets where it is shown dependent on DN in a technical table for every control valve. Please follow the link below.
http://district-heating.danfoss.com/products/motorised-control-valves/range/

Special stainless steel seat and cone prevents erosion and cavitation phenomena. Seat and cone are also guided what means less vibrations and better sealing.

Soft sealing valves, also known as bubble tight valves, insure no leakage which again leads to huge energy savings. No leaking is also related to no pressure loss, meaning the pump does not have to work all the time.

Patented construction of large VF3 valves DN 200; DN 250 & DN 300 have soft sealing construction and have therefore much better sealing than less performed metal to metal valve types.
Danfoss large valve have beside of main A-AB port also soft sealed B-AB port.

We have two types of actuators. One type (AMV(E) 685) has 5.000N and another one (AMV(E) 855) 15.000N.

We are just in testing procedure to proof what we think. As mentioned above, also B port is soft sealed and therefore we need to test if soft sealing will create any problems (vacuum). However we plan to make accessory as blind flange for DN 300, screws and instructions how to make 3 port valve suitable to operate as 2 port valve.

Case studies

  • if (isSmallPicture) { Eurasburg; } else if (isBigColumns) { Eurasburg } else { Eurasburg }
    Successful transition from oil boilers to a local heating network in Eurasburg

    In the Wittelsbacher Land near Augsburg the local network in Eurasburg supplies heat to 80 buildings using a wood chip heating system. Danfoss’ substations ensure efficient heating in all building types, and its modern SCADA solution enables remote system monitoring and management. 

  • if (isSmallPicture) { Rothes CoRDe plant; } else if (isBigColumns) { Rothes CoRDe plant } else { Rothes CoRDe plant }
    DrivePro® Lifecycle Services secure maximum uptime for Rothes CoRDe

    SCOTLAND: The Rothes CoRDe plant, a biomass-fired combined heat and power (CHP) plant, ensured maximum uptime thanks to several DrivePro® Lifecycle Services.

  • if (isSmallPicture) { ; } else if (isBigColumns) { } else { }
    Intelligent optimisation of district energy in new residential apartments

    Two new build apartments in Docklands, London and Newbury Racecourse, Berkshire have been equipped with intelligent Danfoss solutions, bringing increased control and stability as well as greater than 20% peak energy reduction.

  • if (isSmallPicture) { In Helsinki a total of 667 addresses in a mix of large and small buildings and apartments have had the Leanheat software installed.; } else if (isBigColumns) { In Helsinki a total of 667 addresses in a mix of large and small buildings and apartments have had the Leanheat software installed. } else { In Helsinki a total of 667 addresses in a mix of large and small buildings and apartments have had the Leanheat software installed. }
    Leanheat makes buildings smart

    In Europe, 30 percent of all energy consumption goes to heat or cool buildings. Danfoss has the solution to lower energy usage and improve indoor climate by adding a digital element: Leanheat software.

  • if (isSmallPicture) { MS Cinderella saves more than 1000 tpa marine diesel with new ventilation control; } else if (isBigColumns) { MS Cinderella saves more than 1000 tpa marine diesel with new ventilation control } else { MS Cinderella saves more than 1000 tpa marine diesel with new ventilation control }
    MS Cinderella saves more than 1000 tpa marine diesel with new ventilation control

    Aboard the Viking Lines cruise ship M/S Cinderella, Danfoss AC variable speed drives are delivering fuel savings so large that the cost of installing the drives will be fully recovered in less than eighteen months.

  • if (isSmallPicture) { Solar heating plant reduces CO2 emissions by 15,700 tonnes annually; } else if (isBigColumns) { Solar heating plant reduces CO2 emissions by 15,700 tonnes annually } else { Solar heating plant reduces CO2 emissions by 15,700 tonnes annually }
    Solar heating plant reduces CO2 emissions by 15,700 tonnes annually

    The world’s largest solar heating plant in Silkeborg, Denmark harnesses energy to heat the homes and workplaces of 40,000 citizens. It supplies 18-20% of the annual heat consumption in the city of Silkeborg, Denmark, which has an ambitious target of CO2 neutrality in heat production by the year 2030.

Videos