• My Apps
    My Apps You will have the option to use My apps once you login.

New ‘Smart Store’ paves the way for 21st century supermarkets

Thursday, 29 June 2023

New “Smart Store” will work as Danfoss’ test centre for energy efficiency technology.  ‘The Smart Store’ is expected to be approximately 50% more energy efficient compared to a typical supermarket with a first-generation CO2 refrigeration system.

New flagship “Smart Store” supermarket in Nordborg, Denmark:

  • Runs off sustainable energy sources
  • Reuses the excess heat created by cooling cases, reducing supermarket heating costs by up to 90%
  • Not only operates as a functioning supermarket, but is also a development centre for testing new technology

As the world’s population continues on its course to reach 10 billion people by 2050, investments in sustainable food retail and storage are urgently needed to ensure we are able to feed the growing number of people on the planet. The pressure is growing, both on energy demand and costs, and on the need to cut down on food loss. If food waste was a country, it would be the third largest emitter behind the US and China, contributing to up to 10% of the world’s greenhouse gases.

To address these problems directly, Danfoss is today announcing the opening of a new, flagship supermarket which is expected to be approximately 50% more energy efficient compared to a typical supermarket with a first-generation CO2 refrigeration system and no energy efficiency solutions. It is also expected to be approximately 20-30% more efficient than an equivalent local store already fitted with multiple energy efficiency solutions.

Climate-friendly, super-efficient and loaded with automation solutions, the new ‘Smart Store’ is providing inspiration for food retailers in a world of rising energy costs, emissions, and worsening food losses.

 

Commenting on the launch, Jürgen Fischer, President, Danfoss Climate Solutions, said: 

While supermarkets and retail food stores are an integral part of communities around the world, they are also big energy consumers. The average profit margin for a large food retailer is just 1.7%, which puts every operating cost under scrutiny. Energy is an area where significant savings can be achieved with relatively low investment and good payback times. In fact, the US EPA estimates that one US dollar (£0.80, EUR 0.90) in energy savings is equivalent to increasing sales by US$59 (£47, EUR 54).

The range of new solutions in the ‘Smart Store’ demonstrate the significant savings that can be achieved in supermarkets, with a typical payback time of under 3 years. By using world-class heating and cooling technology, the new supermarket will waste less energy and less food and will show the journey to a zero emissions supermarket.

The Smart Store supermarket demonstrates that it’s not only possible to design and build an energy-efficient supermarket with solutions available today, but it also makes good business sense. 

Solar power is the supermarket’s primary energy source with 100 kW solar panels on the building’s roof providing green energy to support the supermarket operations.

Heat capture and reuse is also key to the energy efficiency of the supermarket with up to 90% reduction in supermarket heating costs expected. Excess heat is the world’s largest untapped source of energy. The ‘Smart Store’ is fitted with state-of-the-art heat recovery units, designed to recover the waste heat from all the refrigeration systems. The recovered heat is reused to heat up the store and produce domestic hot water, with any additional heat shared with residents of the surrounding town through a district energy network. 

Other initiatives such as installing doors on refrigerator and freezer cases will save around a third on energy use, while the choice of LED lighting uses up to 85% less electricity than incandescent bulbs. Automation and monitoring of the ‘Smart Store’ adds another layer of energy saving.

Jürgen Fischer added: “Danfoss has reimagined what food retail stores could look like in the 21st century. For the first time, all of Danfoss’ most cutting-edge technology and energy efficient food retail solutions are being brought together into one retail site. But the new Smart Store supermarket is only the beginning. Because it will also serve as an Application Development Centre, a ‘live’ testing site for new technologies which we hope will inspire food retailers around the world to move towards zero emissions supermarkets – while making economic sense.”

 

For further information please contact:

Amanda Chick, Global PR Lead
Ph: +357 9514 5470
Email: amanda.chick@danfoss.com 

Danfoss Smart Store ADC demonstrates the journey towards a net-zero supermarket