Estonia’s border authorities have launched a hybrid patrol vessel that both protects the environment from oil spills and cuts fuel consumption thanks to innovative hybrid electric propulsion from Danfoss Editron. The 45-metre ship built by Baltic Workboats is equipped with Editron hybrid electric drivetrain systems, allowing efficient and quiet electric cruising and a swift, powerful reaction to emergencies.
The wave-piercing patrol ship will be used by the Estonian Police and Border Guard Service, mainly for use in combating pollution threats. It is the largest patrol vessel ever built by Baltic Workboats (based in Saaremaa, Estonia), and the first in the firm’s emerging range of battery hybrid patrol ships.
The vessel contains an Editron marine system, which is half the size of a conventional diesel-electric propulsion and power plant system, making it the most compact on the market today. The system’s highly-efficient and lightweight Danfoss Permanent Magnet Machines reduce fuel and running costs, significantly reducing both payback period and CO2 emissions. The control and monitoring software, and the control systems are all integrated into one single system made by Baltic Workboats.
Peeter Raamat, Head of Technical Department at Baltic Workboats explained: “We looked into the operating profile and decided this would be an excellent project to build as a hybrid vessel. We chose to work with Danfoss Editron due to the fact that it is a very flexible and very good system. Also, the size of equipment is very small. This is really important for the ship builders because there is never enough space.
The needs of the patrol boat made it an excellent project to build as a hybrid vessel. For example, the hybrid electric benefit of engine redundancy is important for the Estonian Coast Guard — in case of engine failure, you can switch to diesel-electric or batteries — while you also have improved fuel efficiency, and much lower noise levels in diesel-electric and fully-electric modes when compared to big diesel engines, which is a big benefit for the crew.”
While the ship will also be used for patrolling, firefighting, and search and rescue missions in Estonian waters, its main role will be monitoring and responding to pollution threats, using state-of-the-art radar that can detect surface contamination, such as oil spills, from up to five miles away. The Editron propulsion lets it leap into action with a top speed of 27 knots, while the fully-integrated energy storage system allows electric cruising at typical working speeds of up to 10 knots. The Editron marine systems’ extremely low vibrations and noise also give the patrol boat the ability to run in stealth mode while carrying out anti-smuggling operations.
Ahto Mägi, Boatswain of Raju, helped rescuing more than 400 refugees in the Mediterranean on his former ship, and for him multi-functionality is the most important ability of a vessel: “The first impression for me about the ship is that it is really fast.”
Jani Hartikka, Project Manager at Danfoss Editron commented: “The specialty of the ship is the flexibility between the operational modes. In full electric mode the vessel can go up to 10 knots without engine noise or vibrations. When you are mooring somewhere during nighttime, the energy consumption is very low, and you can sleep in a quiet vessel. Which is unique. At least from a crew’s point of view.
With changing regulations, I see that the demand for such hybrid electric solutions will grow rapidly in the near future as ship owners switch to electrical vessels to reduce their CO2 emissions. Creating this unique vessel together with Baltic Workboats already puts us on the front line of development.”
In this case, the patrol boat’s ability to run cleanly and quietly means that it is already prepared for stricter environmental regulations, while its Editron marine systems’ durability and shock-resistance make it well-suited to the extreme conditions faced on open waters in the Gulf of Finland.