• My Apps
    My Apps You will have the option to use My apps once you login.

Peter Taboada tailors energy-efficient wellboat SWRO with flexible Danfoss technology

Wednesday, January 17, 2024

Peter Taboada works closely with wellboat builders to meet their water-making needs.

Peter Taboada has been a pioneer in designing and producing SWRO plants for wellboats and works closely with shipbuilders and shipping companies to meet their water-making needs. With extensive experience in the marine sector, the Spanish water treatment specialist’s approach focuses on reliable energy efficiency that makes optimal use of available space to maximize their customers’ return on investment (ROI).  Flexible Danfoss high-pressure pumps and energy recovery devices are part of the company’s success. 

Peter Taboada’s extensive experience in the marine sector led to its involvement in some of the first wellboats built for delousing salmon with freshwater treatments.

“SWRO plants for wellboats are similar to many other marine projects,” says Peter Taboada’s marine sector manager, Jacobo Perez.  “However, due to wellboat design and the quantities of fresh water that operators need to produce, making maximum use of minimum space is even more critical. And because wellboat operators don’t make money when their vessels are in port for maintenance, near-constant uptime and system reliability are a must. Finally, of course, energy efficiency is essential for both financial and environmental reasons.”

“Because of all of these factors, we approach each wellboat project with fresh eyes. We work closely with shipbuilders, wellboat operators and our vendors to maximize the ROI of every wellboat SWRO plant. Rather than one-size-fits-all plants, we try to meet or exceed customer requirements by customizing each design to the specific conditions. Often, these solutions can produce more water, more flexibly than the original brief stipulated.”

To meet these challenges for its latest two wellboat projects, Peter Taboada’s engineers designed a two-train 5000 m3/day SWRO plants based on Danfoss technology. Each 2500 m3 train builds on two APP 65 high-pressure pumps and two iSave 70 energy recovery devices.  

“Danfoss’s range of compact components works well with modular designs,” says Perez. “In addition to energy efficiency, Danfoss pumps and ERDs are also known for their reliability and long service intervals. When this dependability is combined with the system redundancy enabled by a multiple-train design, operators are ensured of consistent supply in almost any situation. This assured uptime is a big advantage for wellboat operators who invest heavily to serve the salmon industry.”

At the time this case was written, the Spanish water-treatment specialist had already completed four wellboat projects, including this and two other                5000 m3/day plants and one 3000 m3/day plant. The next two, which will be commissioned in 2024, will have even higher capacities of 15,000 m3/day and 10,000 m3/day.  

“We have also specified Danfoss high-pressure pumps and ERDs for these latest projects,” explains Perez, “and we continue to work with them after the plants are up and running. We monitor our plants remotely to constantly improve service and maintenance. Danfoss components and people make this easier. We share data with them, and they share their insights with us so we can both better understand trends proactively. Everyone is prepared for success but not necessarily for problems. This is how you measure the quality of your partnerships – when there is a problem, partners need to move fast to solve it, and we can count on Danfoss to do this.”

Related products

  • if (isSmallPicture) { APP high-pressure pumps - Danfoss; } else if (isBigColumns) { APP high-pressure pumps - Danfoss } else { APP high-pressure pumps - Danfoss }
    High-pressure pumps for SWRO applications

    The range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.

  • if (isSmallPicture) { iSave energy recovery device - Danfoss; } else if (isBigColumns) { iSave energy recovery device - Danfoss } else { iSave energy recovery device - Danfoss }
    iSave® energy recovery devices for high-pressure membrane applications

    With a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day

Download the case study as PDF