• My Apps
    My Apps You will have the option to use My apps once you login.

APP pumps with ceramic chosen for containerized solutions

Thursday, June 20, 2024
Gefico chooses Danfoss ceramic APP pumps and iSaves for modular SWRO solution

Gefico chooses Danfoss ceramic APP pumps and iSaves for modular SWRO solution

Gefico engineered an energy-efficient 750m3/day SWRO train for a customer who needed both containerized and skid-based solutions for seven trains at three different Jamaican resorts. Danfoss APP ceramic pumps and iSave ERDs are at the heart of the compact, modular trains with an SEC of just 2.36 kWh/m3.

When a Spanish engineering company needed one compact, reliable, and energy-efficient SWRO solution for three separate end users, Gefico’s engineers proposed a compact, modular train design that could be both containerized and built on skids. Danfoss’s ceramic APP pumps and iSave ERDs are at the heart of the seven trains that Gefico designed and produced.

Gefico’s customer, Estel, is a Spanish engineering company that provides build-own-operate (BOO) SWRO, wastewater, and electricity-generation solutions for hotels and resorts worldwide. Estel approached Gefico in Spring 2023 with an interesting request for a proposal. How would Gefico design a solution that Estel could utilize in Jamaica, where it needed BOO SWRO plants for three different resort customers, two of whom required containerized plants with a 1500 m3/d capacity, and one of whom needed 2250 m3/d for an existing building?

According to Gefico’s sales director, Javier Expósito Pernas, the project perfectly fits Gefico’s decades-long experience in the marine, offshore, and land based SWRO sectors. “Maximizing output per cubic meter of plant space was, of course, a critical starting point because two of the end users needed containerized solutions. At the same time, all plants had to provide remote monitoring and the robustness to deal with Jamaican seawater’s particulate levels. Finally, and very importantly, Estel has extensive experience with BOO, so they think consistently in terms of total costs of ownership. Consequently, they thus also required excellent energy efficiency and operational reliability to enable predictably low energy and maintenance expenditures.”

To comply with Estel’s multi-faceted requirements, Gefico’s engineers designed a modular system based on a compact 750 m3/d train that could be flexibly combined in multiple ways. Two trains in one 40’ container would be ideal for each of the two resorts that required 1500 m3/d. Three trains could be built on skids for easy transportation to the third resort with the existing building that required 2250 m3/d in all. Each of the seven trains is built around a Danfoss APP 38 ceramic high-pressure pump and an iSave 40 ERD, and all are equipped for remote monitoring.

“Our modular design has several significant advantages,” explains Pernas. “The modularity gives flexibility and scalability, which reduces CAPEX related to design and production costs, but also lowers OPEX by standardizing components and streamlining maintenance and spare parts procedures. At the same time, redundancy is built into each of the three plants, which further simplifies maintenance and is critical risk mitigation for resorts that depend on consistent fresh water supplies.”

Gefico commissioned the first modular plant in early May of 2024, just under 12 months from Estel’s RFP. The following two are scheduled to come online soon after.

“Danfoss HP pumps and ERDs are a key part of this modular solution,” concludes Pernas. “Not only is their compact footprint ideal for tight spaces like these, but their energy efficiency and reliability are unparalleled. The combination of APP and iSave technology enables us to achieve an SEC of 2.36 kWh/m3, so both Estel and their customers can minimize the financial and environmental costs of their SWRO.”

“That we now have the option of installing ceramic versions of the APP pumps is also a real plus in some remote locations, for example these in Jamaica. Danfoss’s long service intervals and remote monitoring capabilities help both Estel and us further improve our ability to minimize operational costs and downtime. And their stock policies and short lead times make it possible to build and deliver customized solutions like this with predictable speed.”

Related products

  • if (isSmallPicture) { APP high-pressure pumps - Danfoss; } else if (isBigColumns) { APP high-pressure pumps - Danfoss } else { APP high-pressure pumps - Danfoss }
    High-pressure pumps for SWRO applications

    The range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.

  • if (isSmallPicture) { iSave energy recovery device - Danfoss; } else if (isBigColumns) { iSave energy recovery device - Danfoss } else { iSave energy recovery device - Danfoss }
    iSave® energy recovery devices for high-pressure membrane applications

    With a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day

Download the case study as PDF