Welcome efficiency. Welcome electric.
The electrification megatrend will increase electricity demand by 150%. To prepare, the EU has therefore set a target of 40 GW electrolyzer capacity by 2030, equivalent to approximately 200 TWh electricity consumption. Hydrogen is the bridge between renewable electricity and hard-to-decarbonize sectors, which can help society meet this electricity demand, sustainably.
Enabling a future powered by electricity
To achieve an electrified world, industry requires solutions that maximize energy efficiency from renewable sources when capacity is high and convert into firm clean energy for use when capacity is low. That requires high efficiency power conversion with low harmonic distortion while ensuring global scalability and cost-effectiveness.
In its pure form, hydrogen can be used to replace fossil fuels in some industries. To e-fuel even more industry, the hydrogen can be synthesized into e-methanol, e-ammonia, or e-diesel. By converting to these sustainable energy sources, we can reduce reliance on fossil fuels.
Source: Adapted from Ørsted & EU data, approximate numbers
Electrification of energy consuming sectors is vital for decarbonization
Our ambition is to help you achieve your electrification goals. Because together we can create a sustainable future powered by electricity. As a world leader in electrification as well as in heating and cooling solutions, we here at Danfoss are always thinking holistically on topics such as Power-to-X. Coupled with state-of-the-art co-development facilities and an inherent engineering mindset, our employees are always eager to share their knowledge to find the best solution to the challenge at hand. With a core focus on energy efficiency and system effectiveness, Danfoss is ideally placed as your expert partner in Power-to-X, both technically and commercially.
Recognized world-wide as a reliable supplier, Danfoss adheres to the highest international standards in production and development quality. With Danfoss solutions you get proven competitiveness and reliability, to get your business on target for a decarbonized economy.
Events
Our approach
At Danfoss, we help you think beyond the system itself. By taking a holistic perspective on the entire ecosystem, we secure energy efficiency and system effectiveness that is both scalable and economically viable. With extensive expertise in Power-to-X systems and electrolysis, we tailor the solution to your specific needs. That way you get a plug-and-play system with maximum performance that evolves alongside your operations, at your pace. Danfoss technology has been developed and refined to deliver future-proof, guaranteed performance with many added features to lower risk and ensure a stable operation. You achieve better total economy and peace of mind for operational excellence of your electrolysis plant. Danfoss will provide you a grid-friendly, approved solution with impressive energy efficiency. Low harmonics and a high power factor ensure that you have a competitive power supply for your electrolyzer at hand. With long experience in power conversion combined with a leading position in the world, Danfoss is your ideal partner for your investment in the hydrogen market.
Where there is energy, there is opportunity
Coupled with state-of-the-art test facilities and an inherent engineering mindset, our employees are always eager to share their knowledge to find the best solution to the challenge at hand. Together with a core focus on energy efficiency, not only in the products we deliver but also holistically in entire systems, Danfoss is ideally placed as an expert partner in Power-to-X.
Recognized world-wide as a reliable supplier, Danfoss adheres to the highest international standards in production and development quality. One example: our drives for power conversion are produced and developed according to the stringent requirements of the automobile industry.
Contact our experts
Keen to get started?
Are you ready to accelerate your electrification journey? Our Power-to-X expert, Helge Vandel Jensen, is ready to get in touch with you and have an informal discussion.
Learn more
Stay up to date with Danfoss Drives
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Introducing the DrivePro® Circularity Claim stickerMonday, May 6, 2024
With the new DrivePro® Circularity Claim sticker, you receive instant confirmation that an AC drive has successfully undergone the DrivePro® Start-up commissioning service and has been configured to provide optimum efficiency and performance
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }Unlocking Innovation: Exploring the Power of Interdisciplinary CollaborationFriday, May 3, 2024
On 9th of April 2024, a remarkable event unfolded at Danfoss Vaasa premises, bringing together the Veturi companies in Vaasa region: Wärtsilä, Mirka and Danfoss under one roof for a collaboration event
-
if (isSmallPicture) { ; } else if (isBigColumns) { } else { }iC2-Micro is now easier to program and has UL LZGH2/8 certificationWednesday, March 27, 2024
Now you can program iC2-Micro even when it is disconnected from power supply, using a new quick adapter. The integrated smart logic controller (SLC) gives flexibility and a less complex installation. Since the drive is UL LZGH2/8-certified, you enjoy a simpler system certification process for use in HVAC/R systems with A2L refrigerants. With power range up to 22 kW, this drive serves even more applications.